This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Active Beam forming for 4 Tx of AWR1642 using Time Delay Block (Because phase shifter is not available on the current EVM board)

Part Number: AWR1642BOOST

Because there’re no phase shifter in the current EVM board, so I’m thinking about using the time delay to achieve beam forming. But what I wonder is that when I want to make the phase of signal impinging on 4 RX the same by adding some time delay, then these amount of time are so tiny as I calculated in the figure below (roughly 2.6485.10-11 which is equivalent to 10^-5 an ADC sampling time) so I just concern this value is too small to use fractional delay . Therefore I want to ask is it possible to achieve beam forming by this way, and could you me offer me some advice and source code if available. Thank you so much!