Other Parts Discussed in Thread: FDC2114EVM
HI
I am using FDC2212. I want to trigger the MCU via the INTB pin interrupt and read the data register of the FDC2212 via I2C. When initializing the FDC2212, set the ERROR_CONFIG register to 0x0001; the CONFIG register is set to 0x1601. After setting, is the INTB pin output when the data of channel 0 and 1 is ready? If there is? time? INTB pin level? INTB pin output voltage size? if there is not? How to set up registration?
BestRegards
Sun