This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a custom mmWave radar PCB utilizing an XDS110 very similar to the AWR1443BOOST in a different form factor. When I attempt to load the radar image files using UniFlash, the associated COM port locks up. This is what the console looks like when this occurs:
Cortex_R4_0: Initialization complete.
Cortex_R4_0: Flashing process starting...
Cortex_R4_0: Connecting to COM port COM10...
Cortex_R4_0: Reset connection to device
Cortex_R4_0: Set break signal
I have verified that the SOP configuration is correct. Any help would be much appreciated.
Regards,
Brendan
Hi Akash,
I believe the problem is with my flash chip not running in Quad mode. The flash chip on the AWR1443BOOST is no longer recommended for new designs so I am using the following component:
S25FL064LABNFV040. It does not default to Quad mode and I need to write to it via UART on the AWR1443. My design has an XDS110 emulator on board just like the AWR1443BOOST. I was hoping to utilize the RS232 connection from the XDS to the AWR1443 chip in order to program the flash into Quad mode.
Any thoughts? I will work on getting pictures of the board but may take some time to get approval from my customer. Thanks in advance.
Regards,
Brendan
Hi Akash,
Thanks for the quick response. Unfortunately these were not my issues. COM10 is the UART port:
The SOP jumpers are in the correct position. I traced the voltage from the header pins to the AWR1443 pins to confirm that my design was not the issue. SOP seems to checkout.
Can I use the USB interface (COM10) to write to my serial flash via the AWR1443 chip? I believe I need to put the flash in Quad mode.
Regards,
Brendan
Hi Joe,
Thanks for the response. The Errata document lists the S25FL132K0XNFB010 as one of the devices. This device is close to obsolescence so I investigated the replacement from Cypress. You will see in the following image the drop-in replacement for the S25FL132K0XNF family is the S25FL064LABNF family.
Do the AWR1443BOOST eval boards need to set the flash into Quad mode at the factory before shipping out?
Thanks,
Brendan