This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDC1000-GASEVM
Hello! I have a set of TDS1000-TDC7200EVM and TDS1000-GASEVM. I started to remake the electronic Board TDS1000-TDC7200EVM to measure the flow as well as using TDS 1000-GUSEVM. I replaced (С27, S32), (С36), (С42, С43), (39, 46). I have installed (R5), (JP6). I deleted R41, R42. I did the steps according to SV601158-001_REV B_BOM. I did not change only the Y2, left it equal to 8 MHz. I want to know what steps will lead to the fact that the cost of electronic TDS1000-TDC7200EVM will be equivalent to the TDS1000-GUSEVM. I want to make the changes to the end so that we can measure. I plan to measure in CPU with 122 kHz sensors. Is it critical to leave Y2 unchanged? Please give a detailed answer, thank you in advance!