Hello,
Is it possilble to use AWRxxx radar sensor to detect distance to static objects in a tunnel? For example tunnel about 6m width and 4m height. I would like to detect an free space in front of the radar in distance up to 10m. Any objects/obstacles in that space I would like to detect with an accuracy of a few centimeters. Radar would be in a fixed position, or move slowly. Is it possible to use AWRxxx radar in such conditions?
Thanks in advance.