This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Creating Serial port to read ADC data using CCS

Part Number: AWR1642BOOST


Hey,

I have been able to read the ADC data using CCS and tera term. But, I want to configure AWR1642Boost board using MATLAB instead of the term term.

I have created the serial port, but don't know how to configure the parameters like I did in Tera term.

Is there a guide available to do so?

Many Thanks

 

  • Command should be in ASCII format and send to device ending with '\n' so that device gets to know the termination of single command string.
    And while you are sending a CLI command from TeraTerm or Matlab, you can check the UART content device recieves.

    Try to debug using CCS and put breakpoint in utils\cli\src\cli.c: CLI_task(..) function where it reads UART data (UART_read..) and after reading it parses it and further call related APIs.
    You can do experiment by sending CLI message from Matlab and check if it reaches to device as epxected (in above mentioned function).


    Regards,
    Jitendra
  • Thanks Jitendra.

    1) "While you are sending a CLI command from TeraTerm or Matlab, you can check the UART content device recieves". How can we check this?

    2) I have written a script in MATLAB, it runs successfully but nothing happens in the CCS output screen.

    In the CCS output screen, I just see:
    [Cortex_R4_0] Debug: Launched the Demo Initialization Task
    Debug: UART Instance @0800b2b8 has been opened successfully
    Debug: UART Instance @0800b2c4 has been opened successfully

    These messages are displayed when I run the processors after loading the firmwares.

    3) When using tera term, in the start, I choost the option of MSS. How can it be done in MATLAB.

    4) Also, after using 'sensorStart' command in tera term, a message is displayed in output screen of CCS that configuration successful. But once the script in MATLAB is run, I do not see any change in CCS. May be its because data is not captured, or connection with CCS is not made. I am not sure tough.

    MATLAB script:
    Port_info = instrfind('Port','COM3');
    newobjs = instrfind;
    fclose(newobjs);
    newobjs1 = instrfind;
    clear CCS_port
    CCS_port = serial('COM3');
    set(CCS_port,'BaudRate',115200)
    set(CCS_port,'DataBits',8)
    fopen(CCS_port)
    newobjs1 = instrfind;
    %after this, port is opened

    fprintf(CCS_port,'flushCfg \n');
    fprintf(CCS_port,'dfeDataOutputMode 1 \n');
    fprintf(CCS_port,'channelCfg 2 1 0 \n');
    fprintf(CCS_port,'adcCfg 2 1 \n');
    fprintf(CCS_port,'adcbufCfg 0 0 1 1 \n');
    fprintf(CCS_port,'profileCfg 0 77 20 5 80 0 0 40 1 256 6000 0 0 30 \n');
    fprintf(CCS_port,'chirpCfg 0 0 0 0 0 0 0 1 \n');
    fprintf(CCS_port,'frameCfg 0 0 128 1 20 1 0 \n');
    fprintf(CCS_port,'lowPower 0 0 \n');
    fprintf(CCS_port,'sensorStart \n');
    out = fscanf(CCS_port)
  • Can you also please explain how to perform this step in a bit more detail:

    Try to debug using CCS and put breakpoint in utils\cli\src\cli.c: CLI_task(..) function where it reads UART data (UART_read..) and after reading it parses it and further call related APIs.
    You can do experiment by sending CLI message from Matlab and check if it reaches to device as epxected (in above mentioned function).

    I have located the point, but how should I put the breakpoint?
    /* Read the command message from the UART: */
    UART_read (gCLI.cfg.cliUartHandle, &cmdString[0], (sizeof(cmdString) - 1));

    What should I change it into?

    Many Thanks
  • Never mind, I have been able to do it by amending the script I pasted above. It works fine now.
    Thanks a lot...