Other Parts Discussed in Thread: HDC2010
Hi
Question:
Can the EVM GUI with HDC2010EVM be used also with a sensor (HDC2010) with the "other" ADDR (namely 1000001) ? the HDC2010 arrives with ADDR 1000000 (ADDR node connected to GND via R12)
I'd like to Evaluate the two addresses together or at least one at the time; I've changed the address by connecting ADDR to VDD (removed R12, moved it to R4) ==> sensor is not usable with the GUI
connected the two sensors as a BUS enabled the communication to device ADDR 1000000 with operational GUI (not surprising)
so again: is there a way to modify in the GUI and enable the communication to work with the "second" device or two as a BUS?
thanks
-ron