Hi,
I followed the instructions in this e2e thread ( ) in order to bypass the CLI and have an embedded configuration of the RF front-end. This seems to work, as I get the terminal output on the DATA UART port (seeing the magic word etc., so I suppose the data is correct), if using TeraTerm for example.
Is it still possible to visualize the data using the PLOT tab of Demo Visualizer? What needs to be done to enable this?
Background is that I would like to have the same or slightly different configuration on several AWR1642BOOST EVMs by flashing them with the same or different FE configs and let them work by themselves. I do not want to have the need to connect a Laptop to download the configs to the device on every reset of the device.
But on the other hand I would still like to have the opportunity to connect to any of the EVMs and check it is proper function by looking at the PLOT tab, seeing objects etc.
Many thanks and best regards,
Gregor