This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1080: HDC1080/50 failures

Part Number: HDC1080
Other Parts Discussed in Thread: HDC1050,

Hi,

I have had several cases where a HDC1080 or HDC1050 humidity sensor has failed. The failed sensors have a low resistance short between VCC and GND, and in one case the I2C SCL pin also had a short circuit to ground.

These sensors are mounted on bare prototype PCBs that are used for SW development so ESD is certainly a possible cause as is physical damage to the sensor element (although no damage to the sensor is visible).

Can minor damage to the exposed sensor surface lead to a short circuit in the sensor?