This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM60-Q1: minimum Setup time for Vout of LM60-Q1

Part Number: LM60-Q1


Hello Apps team, 

My customer is asking minimum setup time of LM60-Q1 after supplying input voltage. 

Figure 11 in datasheet shows output voltage which represents temperature is set within 5us after power supplied.

Vo is read as 0.8V, so it would be around 60'C with calculation.

Can I assume the voltage read after power supply 5us is correct Vout which reflect current temperature?

What can be minimum setup time if voltage reading should be waited for more?

Thank you in advance.