Other Parts Discussed in Thread: MMWAVEICBOOST,
Hi there,
I am using IWR6843ISK with the MMWAVEICBOOST. I am currently using the mmWave demo visualizer, but I found a problem.
From the plot, it seems that the sensor only detected objects when it is moving but did not show when it is static. I have made sure that the clutter removal is disabled when configuring the sensor. Following is the .config file I download from the visualizer.
% ***************************************************************
% Created for SDK ver:03.01
% Created using Visualizer ver:3.1.0.1
% Frequency:60.25
% Platform:xWR68xx
% Scene Classifier:best_range_res
% Azimuth Resolution(deg):15 + Elevation
% Range Resolution(m):0.047
% Maximum unambiguous Range(m):9.02
% Maximum Radial Velocity(m/s):3.99
% Radial velocity resolution(m/s):0.25
% Frame Duration(msec):100
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% Angle of Arrival FoV: Full FoV
% Range FoV: Full FoV
% Doppler FoV: Full FoV
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 60.25 50 7 53.57 0 0 70 1 224 4915 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
frameCfg 0 2 32 0 100 1 0
lowPower 0 0
guiMonitor -1 1 1 0 0 0 1
cfarCfg -1 0 0 8 4 4 0 1280 1
cfarCfg -1 1 0 8 4 4 1 1280 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.42
cfarFovCfg -1 1 -4 4.00
sensorStart
Any help would be appreciated.
Thanks in advance