Hello All,
My customer is working on a new low-cost pH measuring device. Currently the measurement stage is done with a quadruple operational TLC2264ID in SOIC-14 package.
Customer has the problem that at 50 °C the bias current Ib causes the measurement to drift when they supply the signal with pH simulator with impedance equal to 1Gohm.
Customer has tested a competitive tool and it does not have this drift, and the measurement is much more stable.
The competitive tool uses another operational amplifier which has a compensation function that keeps the Ib constant at 5pA up to 85 ° C.
Customer at the beginning was looking for an OpAmp to replace this competitive p/n.
But now customer is more focus on specific p/n similar to LMP91200 for pH sensing.
Do you have a comment here?
Many Thanks,
Antonio