This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5013-Q1: Max of Tr and Tf at pin "OUT"

Part Number: DRV5013-Q1

Hi

What is the maximum value of Tr and Tf at pin "OUT" of DRV5013-Q1?

In the datasheet of the device, the tyipcal value is 200ns as Tr and 31ns as Tf.  PLS let me know the maximum value at the same test condtions as shown in below.
  R1=1k ohm, C0=50pF, Vcc=3.3V

Best Regards, Taki