This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2114: Data for smaller Sensor Area

Part Number: FDC2114
Other Parts Discussed in Thread: FDC1004, FDC2214

Hello

I have comfirmed the doc (SNOA940A)

http://www.ti.com/lit/an/snoa940a/snoa940a.pdf

But I would like to know smaller sensor size.

required detection distance : 10cm approx

assumed sensor size : 5 mm x ___mm   (GND size is same.)

distance between sensor and GND : 1.0mm

Could you let me know the length of the sensor size?

I cannot read from the graph(Fig.3) due to the range.

Thank you

Best regards,