This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: IWR1443 - Raw data interface

Part Number: IWR1443

Hi,

I am planning to use IWR1443 to design 77GHz radar system. I plan on getting the raw data from the IWR1443 and do all the processing in FPGA. There are several interfaces mentioned in IWR1443 and it seems to me that the CSI2 interface can provide raw data. However, I am not sure about this  and so i have following questions

(1) Which interface, in IWR1443, should be used to acquire raw data via FPGA?

(2) Are there any design guidelines when acquiring raw data like mentioned above ?

(3) Could you comment on signal swings on the interface used to capture the raw data so that I have to take care that the FPGA can handle such swings ?

Thanks