Other Parts Discussed in Thread: LM50, , LM50-Q1,
Hi,
Is it true that the only difference between TMP235 and LM50 is the voltage supply range?
The output voltage vs. temperature equation seems to be the same, and the accuracy is almost the same.
And is it true that we should promote TMP235 instead of LM50 as long as the customer is using 5V or 3.3V to power the temperature sensor?
I can't see any reason to use LM50 instead of TMP235.