This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: How to capture raw data frame by frame from DCA1000EVM

Part Number: DCA1000EVM

I fllow the post to real-time capture rarw data by DCA1000EVM:

https://e2e.ti.com/support/sensors/f/1023/t/826017

and use the example code in

'C:\ti\mmwave_studio_02_00_00_02\mmWaveStudio\Clients\AR1xController\api.h'

The example code shows:

int8_t path[20] = "D:\\adc_data_DCA.bin";
retVal = StartRecordData(path, 1);
// TODO: Handle return error value of above API call

// To stop the capture
retVal = StopRecordData();

in order to record data, I insert sleep() function between start and stop,

but It can't guarantee that I capture data frame by frame.

e.g. I use sleep(20000), I can capture approximately 99.7 frame data rather than 99 frame or 100 frame.

So I want to know there is an api or a way to guarantee that I capture data frame by frame,

or I need drop the decimal part in post progress.

  • Hi

    In the frame configuration you can program the number of frames you want to capture.

    There is no specific API at the mmwave studio level.

    You can also post process as you mentioned

    Thank you

    Cesar

  • Hi Cesar,

    Thank you for your answer.

    I check it, solving this problem in post process is the better way.

    Regards,

    Froglu