This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is there any CCS project example for sending 3d point cloud data over uart?
Thanks,
Vimal
Vimal,
The SDK Out-of-Box Demo provides the example of sending out 3D point cloud data over uart. Please refer to the Out-of-Box Doxygen for more information. The MMWDEMO_OUTPUT_MSG_DETECTED_POINTS has the following structure:
Data Fields
float x
x - coordinate in meters. This axis is parallel to the sensor plane and makes the azimuth plane with y-axis. Positive x-direction is rightward in the azimuth plane when observed from the sensor towards the scene and negative is the opposite direction.
float y
y - coordinate in meters. This axis is perpendicular to the sensor plane with positive direction from the sensor towards the scene
float z
z - coordinate in meters. This axis is parallel to the sensor plane and makes the elevation plane with the y-axis. Positive z direction is above the sensor and negative below the sensor
float velocity
Doppler velocity estimate in m/s. Positive velocity means target is moving away from the sensor and negative velocity means target is moving towards the sensor.
Regards,
Kyle
Hi,
Have you looked at the mmWave SDK demo? the demo sends the point cloud over uart.
The mmWave SDK demo does not include a CCS project spec.
The following thread includes a CCS projectspec for the AWR1843 mmWave SDK 3.1 demo.
https://e2e.ti.com/support/sensors/f/1023/t/760427
You can update it for a later SDK version
Thank you
Cesar