Other Parts Discussed in Thread: PGA460
After the pga460psm-evm device is powered on, how to directly load the data that has been written into the register (or the data in eeprom), that is, how to directly measure the distance using the previously configured data parameters after booting.
For example, after power-on, the configuration parameters of the internal registers and EEPROM are used by default before the P1 or P2 commands are used to test the distance. This process, what steps need to be taken before the ranging command, whether to read the configuration or load the EEPROM, etc.