Other Parts Discussed in Thread: BOOSTXL-PGA460, , PGA460
Tool/software:
Good Afternoon,
I recently evaluated the BOOSTXL-PGA460 and was satisfied with its ability to detect objects at long distances. I decided to use the reference design for the PGA460PSM-EVM and connect it to a different microcontroller on the board but also wanted to add jumpers to connect it back to the MSP430F5529LP to evaluate the board with the GUI if needed. I wanted to make sure that this was a practical way to do this and if so where to connections on the MSP430F5529LP were to to connect the two boards.