This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1010: Sensor accuracy - out of the box, and over time.

Part Number: HDC1010
Other Parts Discussed in Thread: HDC2010, HDC2080

Does the accuracy of this temp/hum sensor deteriorate over time?   Out of the box the accuracy is RH +-2% and DB +-0.2. I use this sensor in my controls and have found the accuracy as stated in the specs.  My problem is the HVAC industry has a study that recommends not using differential enthalpy control for economizers because the sensor accuracy is reported at RH +-5% and DB +- 2 degrees.     I want to try to revise the building code but want to make sure that there is not a calibration issue over the service life that would cause a significant accuracy error.  Thank you.