Other Parts Discussed in Thread: HDC2010, HDC2080
Does the accuracy of this temp/hum sensor deteriorate over time? Out of the box the accuracy is RH +-2% and DB +-0.2. I use this sensor in my controls and have found the accuracy as stated in the specs. My problem is the HVAC industry has a study that recommends not using differential enthalpy control for economizers because the sensor accuracy is reported at RH +-5% and DB +- 2 degrees. I want to try to revise the building code but want to make sure that there is not a calibration issue over the service life that would cause a significant accuracy error. Thank you.