This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear engineer
I am using dca1000evm and iwr1443 boost to collect ADC data, hoping to get the distance, speed and angle information of the target,now I have a few questions about mmwave studio parameter setting. I wish the engineer can help me to answer the questions. Thank you very much.
1. Phenomenon: when I use two TX to collect data, I set the number of chirps in each antenna to 64 (that is to say, there are 128 chirps in a frame), and the idle time is 100 microseconds. At this time, the periodicity is displayed as 40 ms;
When I use three TX to collect data, I set the number of chirps in each antenna to 64 (that is, one frame contains 192 chirps), and the idle time to 7 microseconds. I think the periodicity of the frame should change accordingly, but at this time, the periodicity is still displayed as 40ms, the same as that of two TX;
Question: why does the number of chirps in the frame increase, the idle time is shortened to 7 microseconds, and the frame cycle of setting page display does not change accordingly?
2. According to question 1, when setting the frame parameter in mmwave studio, can I manually set the periodicity at will? For example, set it to 10ms
3. Can I make 256 ADC samples smaller? For example, if it is changed to 100, the amount of echo data will be small. Will it lead to the decrease of accuracy? If you change the number of sampling points, do you need to modify the corresponding other parameters? For example, sample rate (ksps) was changed from 10000 to smaller.
Hello
Your questions seem to be a hybrid of mmWave RF sensing parameter questions and mmWave Device/tool related.
We can help you with device and tool related questions.
For questions pertaining to how chirps affect the sensing capabilities of mmWave sensins please refer to mmWave technology basics.
We have few things that could help you get started :
Introduction to mmWave sensing: FMCW radars
For making a chrip that works well on TI devices please use the following tool
mmWave Sensing Estimator tool under:
We will get back to you with device/tool level answers.
Thank you,
Vaibhva
Hello user5972929,
Frame periodicity is user programmable entity, And it changes the duty cycle of the operation, general guideline is to keep the duty-cycle 50% or lesser mainly from thermal consideration and time needed for post processing of the data.
Programming the Idle time, ADC start time, ramp end time depends upon chirp configuration, For understanding the constrains for this you could refer to the below app-note.,http://www.ti.com/lit/an/swra553/swra553.pdf
For designing the chirp configuration you could refer to mmWave Sensing Estimator tool.
https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/ver/1.3.0/
Yes, you could change the number of samples, This will change the radar system parameters (For example Range resolution),
then you may want to re-adjust slope, sampling rates etc to get back same range resolution, but you may have to trade-off with other parameters. You could refer to below app-note to understand the some of the trade-offs. http://www.ti.com/lit/an/swra549/swra549.pdf
You could refer below link which provides the some of the common chirp configuration for various use-cases (This is developed for using out of box demo application using mmWave SDK framework).
http://dev.ti.com/tirex/explore/node?node=ALYHkY2xyhq2-EgWIUuw-Q__VLyFKFf__LATEST
Thanks and regards,
CHETHAN KUMAR Y.B.