This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
I'm trying to use processor SDK to use the continuous streaming use case on the setup mentioned in the title. I'm following the boot from CCS, however, I don't see a DIP switch settings to apply on the MMWCAS-DSP-EVM board. I would be grateful if anyone can point me to the documentation containing the DIP switch positions for CCS or tell me what it is. The user guide of MMWCAS-DSP-EVM doesn't have boot modes for CCS.
Hi,
I have re-assigned this thread to the correct team.
Sorry for the delay
thank you
Cesar
Dip switch settings can be reviewed using the TDA2x TRM.
http://www.ti.com/lit/ug/sprui29f/sprui29f.pdf
Section:
The switch S4 in the picture [6:1] corresponds to sysboot[5:0]. For CCS, you can put all the switches to 0.