This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can any one suggest a Phase sequence detector IC from TI with the following specification.
INPUT : 3-phase AC 115V @400Hz
FUNCTION : only to detect the Sequence of 3 phase, it should be 0,120,240 phase shift. Don't need to drive any load.
OUTPUT: will not be conneted to any load.
This is an interesting application. In order to make sure that we understand what you are requesting, can you draw the ideal input waveforms and the waveform you wish to create from them. We support the comparator products from TI, and it is possible that we can create what your application requires with a multi-channel comparator.
Chuck
I cannot envision a way to accomplish this with comparators. Comparators would be appropriate for performing zero cross detection of the 3-phase (essentially converting the sine waves to square waves) but this would not help determine if any of the three phases shifted in time. I can imagine that a time to digital converter may be useful in determining if the phases shifted. So I am going to re-route your post to the Sensing team that supports time to digital converters to see if they have any ideas.
Chuck
user6159160,
Our Sensing team only offers a time-to-digital converter for time-of-flight (TOF) applications. The TDC7200 measures the elapsed TOF between a single START pulse and up to five STOP pulses. Unless you are only periodically checking if the phase sequence is correct in a given window of five pulses, the TDC7200 cannot support continuous sampling of the phase. In addition, the TDC7200 was designed to be used in DC systems up to 3.6V supply and input signals. Our team doesn't have experience with or offer any time-to-digital converters specific to 3-phase AC systems.