This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP451-Q1: Drop in replacement and software compatibility with TMP411-Q1

Part Number: TMP451-Q1
Other Parts Discussed in Thread: TMP411, TMP451

We have designs using the TMP411A.  We are making a new HW revision of our systems, but don't want to update the portion of the software that uses the 411. Are the TMP451 and TMP411 drop in replacement compatible on a software level? It looks like the register map is very similar, and the I2C address of the 411A overlaps with the 451A, but I want to check that nothing else has changed.

Regards,

Jackson