This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: 2Tx and Rx error

Part Number: AWR1642BOOST

Hello,

I have a setup of TWR1400, AWR1642BOOST and Devpack. I'm trying to set up 2 antennas and 2 recievers and i follow the steps mentioned in the previose question to do so but i get the following error:

[16:24:14]  [RadarAPI]: ar1.SelectCaptureDevice("TSW1400")
[16:24:14]  [RadarAPI]: Status: Passed
[16:24:14]  [RadarAPI]: ar1.SetupTSW1400()
[16:24:19]  [RadarAPI]: TSW1400 set-up complete.
[16:24:23]  [RadarAPI]: ar1.StartTsw1400Arm("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[16:24:23]  [RadarAPI]: Error:
[16:24:23]  
[16:24:23]  ... MWMCR::EvaluateFunction error ...
[16:24:23]  09-Jul-2020 16:24:23: Frame Config has not been populated,1,
[16:24:23]  Error in => setup_for_triggered_capture_max_30_frames.m at line 6.
[16:24:23]  
[16:24:23]  ... Matlab M-code Stack Trace ...
[16:24:23]      at
[16:24:23]  file C:\Users\mwt\AppData\Local\Temp\mwt\mcrCache8.5.1\Matlab0\Logging\log_status.m, name log_status, line 32.
[16:24:23]      at
[16:24:23]  file C:\Users\mwt\AppData\Local\Temp\mwt\mcrCache8.5.1\Matlab0\MatlabPostPr\setup_for_triggered_capture_max_30_frames.m, name setup_for_triggered_capture_max_30_frames, line 6.
[16:24:23]  
[16:24:23]  
[16:24:23]  Trace:
[16:24:23]     bei MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[16:24:23]     bei MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, MWArray[] argsIn)
[16:24:23]     bei MatlabPostProcGui.MatlabPostProcGUIClass.setup_for_triggered_capture_max_30_frames(MWArray FilePathWithName)
[16:24:23]     bei AR1xController.frmAR1Main.iStartTSW1400IF()

what am i doing wrong?

many thanks

Nilo