Hi,
I am using Part TMP112 and trying to communicate with it through I2C channel, but receives no Acknoledge response back.
I measured all timing parameters and they seems fine.
after start I placed device address 0x90 (A0 is connected to GND), the next clock SDA should acknoledge with low logic but instead stays high.
attached are 2 pictures of the first byte. one with zoom in and one with zoom out. the unit in the pictures are in 100 usec.
and Zoom out:
what can be the reason of why there is no response??
thanks,
Noam Fishman