I'm going to replace Asahi Kasei Micro, AK8771. I suggested mu customer to use DRV5011ADDMRR. They decided to evaluate it.
Then they are facing an issue.Currently #3 pin of AK8771 is connected with Vcc. The datasheet of DRV5011ADDMRR indicates to connect it with GND or Non- connection.
They hope to use the same PCB if they replace it to DRV5011ADDMRR. Then #3 pin of DRV5011ADDMRR is connected with Vcc.
Maximum input from #3 pin
Voltage: 5.5V
Current: +/-10mA
Would you please let us know if they can connect #3 with Vcc?
Please let me know the limited condition when they connect it with Vcc if it's allowed to use on a limited condition.
Are anything happened?
Please advise!!
Look forward to hearing from you
best regards,
Masato Aizu