This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI experts,
I want to design my own hardware system based on the antenna form factor on iwr6843isk EVM, but limited by the size of my PCB, the GND plane around the antenna area can not be fully satisfied? A part of the ground plane and ground via above the antenna will be removed.
So I want to make sure that what is the purpose of the surrounding ground plane in the original design of iwr6843isk? In my design, a part of the ground plane have to be cut off so that the ground plane does not enclose the antenna area. Will this change the antenna parameters and affect the antenna performance.
Regards
Chenhui
BTW: The files that I refer to are here:
swrc355c\swrc355\xWR6843ISK_DesignFiles\Rev_D.
Hello Chenhui,
Ground PTH acts as fence around the antenna. It shields antenna and RF lines from any unwanted interferences. It's difficult to comment but just looking at the structures, impact of the breaking ground shield around the antenna. To be absolutely sure about it's effects on the Antenna performance, Antenna simulations need to be performed.
Thanks and regards,
CHETHAN KUMAR Y.B.