This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using IWR6843 in a new design and I was wondering if you can recommend the ICs that I should use in order to interact with MMWAVESTUDIO and MMWAVEVISUALIZER. The white paper (SPRACP3A) from TI's website states that we need SPI-to-USB and UART-to-USB converters if we do not have access to the 60-pin connector. I thought of using "CP2105-F01-GMR" as the UART-to-USB converter but I could not find the SPI-to-USB converter in "PROC091F(001)_Sch.pdf". Besides the SPI, UART, and MSS Logger signals, are there any more signals I need?
Best,
Julian
Hi,
FTDI device is used for the SPI to UART, you can find this in the MMWAVEICBOOST schematic.
FYI: If you need to process the raw data captured then you need DCA1000EVM, without the DCA1000EVM you can transmit for testing purposes but cannot actual capture and process the data.
Regards,
Charles O