This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: IWR6843 mmWaveStudio Issue

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843, , DCA1000EVM, MMWAVEICBOOST
We are trying to run the DataCaptureDemo_xWR.lua (attached) script on mmWaveStudio for the IWR6843 60 GHz board (picture of setup attached). However, we got some issues with the details below:
Our setup is IWR6843ISK + MMWAVEICBOOST + DCA1000EVM + Ethernet to Laptop. While reading the post processed ADC data (adc_data.bin), we noticed a difference in the range doppler plots between frame 1 and frame 2, which is the expected behavior. However, there is no difference between frame 2 and the rest of the 98 frames. There are 100 frames in total. This is unusual behavior since we had captured data in a controlled environment where a person was moving continuously about 15 meters away from the board. After various debugging (with both the postprocess function in mmwavestudio and our own code to check the data), we have come to the conclusion that there could be an issue with the way the data is streamed in this setup.
It would be greatly appreciated if you could provide us more insight into what the problem could be!. Let me know if you have any questions!
Thanks!