Other Parts Discussed in Thread: MMWCAS-DSP-EVM,
We purchased the MMWCAS-RF-EVM board and MMWCAS-DSP-EVM boards in November 2020, and they have been working fine. In January of 2021 we purchased a 2nd set of boards. Unfortunately, the RF board is not working correctly. One of the 4 radar chips is not synchronized with the other 3. I have attached a Powerpoint file showing images from the 16 Rx channels for one Tx for a data collection. We know this has a problem because we can run the same data collection with the first set of boards and all Rx channels are in sync. We have tested the first RF board with the second DSP board and it works correctly, so we know the problem is with the RF board. This is not a calibration issue because the basic Rx raw data is bad. Is there a fix for this, or do we need a new board?Rx plots for defective board.pptx