Hi,Staff
Please tell me how to calculate Vol (Output Loe Level voltage).
I'm thinking of the following calculation, is there any problem?
Vcc=5V, Output-Pull up =1kΩ, Rds=50Ω
Vol = 5V/(1kΩ + 50Ω)×50Ω = 238mV(min)
Vol = 5V/(10kΩ + 50Ω) ×50Ω = 23.8mV(min)
※It is based on the data sheet Figure 17.
Please tell me how to calculate Vol = 50mV with the following question
e2e.ti.com/.../603195
best regards
cafain