This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP116: FPC Implementation

Part Number: TMP116

Hi team,

My customer is evaluating TMP116 and plans to implement it in FPC. Epoxy adhesive is used to fix the temp sense FPC on detection object. 

There are 2 types of use cases.

a) Epoxy adhesive will cover all the package in 60C temp. condition when implementing, will this damage or erode the package? And operating temp will up to 80C, will this cause overheat problem?

b) We are concerned about the impact on long-term reliability due to distortion or deformation caused by stress when the adhesive adheres to the package or pin. Can this be used for more than 2 years lifetime?

c) Anything else needed attention in these use cases? or do you have any similar application? Could you provide recommended design?

Best,

Zeming

1. 

2.