Dear team,
There are some question on TMP235 accuracy. Please review below question and let me know your opinion.
1. At datasheet 1page and 5page, we can see difference on TMP235 accuracy. which is correct value?
- Datasheet 1paage, ±2.5°C (maximum): –40°C to +150°C (TMP235)
- Datasheet 5page, we found Max +- 2.0°C across a all temp range (–40°C to +150°C) like below. Min/Max value is same between –40°C to +125°C and –40°C to +150°C condition. datasheet typo?
2. About non linearity
- Typ value is +-0.5 °C, Would you let me know min/max value?
- If not, Does accuracy specification include non linearity value?
3. TMP235 transfer value
- Table3, -40°C Ideal linear value is 100mV, piecewise linear value is also 100mV, Is it right that we can see the 80~120mV output result under real system due to +- 2.0°C accuracy?
Thank you.