Other Parts Discussed in Thread: DCA1000EVM, MMWAVEICBOOST, AWR1642BOOST, AWR1642BOOST-ODS, UNIFLASH
Hello,
I am trying to generate a custom version of the demo binary in either the SDK (v3.5.0.4) or the Platform Toolbox (CLI-tool) which enables HW trigger, CLI interface, and streaming LVDS data to DCA1000VEM from the IWR6843ISK. (This follows from my question here https://e2e.ti.com/support/sensors/f/sensors-forum/972898/iwr6843isk-pre-built-binaries-for-iwr6843isk-in-mmwave-studio-cli-tool)
From my understanding, the current binaries allow SW trigger, CLI interface, and streaming LVDS data to DCA1000EVM. I need to simply change the source code to enable HW trigger and compile the binary.
Where in the source code is the SW trigger defined?
I have looked through the mmwavelink code and found the triggerSelect property on line 1006 of rl_sensor.h and I believe we need to change this value to 0x0002 to enable HW trigger mode. However, I cannot find where it is actually defined. I am not sure if I am looking in the correct place and I think mmwavelink may be the framework for passing the commands over CLI, not necessary for the binary installed on the radar. Please direct me to the correct code to change for enabling HW trigger.
Additionally, I have successfully built the binary from the SDK and set up the environment following the user manual.
I believe all I need to do is find the proper code to change in the source code and compile the binary. Please advise.
Regards,
Josiah W. Smith