We have FDC2214PROXSEN-EVM on hand and have below question.
- Is it posible to change proximity sensor to button 1 or 2? our target distance is 5 cm,
- Can we have firmware for debugging purpose?
NT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have FDC2214PROXSEN-EVM on hand and have below question.
- Is it posible to change proximity sensor to button 1 or 2? our target distance is 5 cm,
- Can we have firmware for debugging purpose?
NT
Hi Knighty,
Yes to both questions. If you give me your email, I can send you the firmware.
Thanks,
Rachel
We have one more question.
what is the best connection on the EVM if we would like to evaluate proximity performance by using our own sensor as attached.
I though remove R28 and parallel my PCB sensor with C15, any recommendation?
ThanksProximity.pptx
NT
Hi Knighty,
You don't need to remove R28. You just need to break off the EVM sensors and attach your custom ones to whichever channel you want to use.
Thanks,
Rachel
Rachel,
Yes, it's FDC2214PROXSEN-EVM. we use our own sensor, 2 side PCB as sensor( see attached), we like to detect only one side (top or bottom) only. Do you have any commend on how connect our sensor to this EVM?
Thanks,NT4428.Proximity.pptx
Hi Rachel
I would also like a copy of the FDCProxsen-evm source code and the fdc2214evm Boards
Hi Rachel
I would also like a copy of the FDCProxsen-evm source code and the fdc2214evm Boards
dan@didja-do.com
Hi Dan,
You can order the FDC2214EVM boards from the e-store online. I can send you the PROXSEN-EVM source code via email.
Thanks,
Rachel
hi Rachel,
Will you please send me the firmware for the FDC2214PROXSEN-EVM? I have one and i want to modify it for my application. My email is zhizhuo.wu@cornellcookson.com. Thank you.
Zhizhuo