Hi:
In THVD14X9 datasheet ,Current During Operation: < 3 mA .
Could I use AVDD of PGA900 as power supply of THVD14X9?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
In THVD14X9 datasheet ,Current During Operation: < 3 mA .
Could I use AVDD of PGA900 as power supply of THVD14X9?
thanks
Hello,
The AVDD regulator can supply up to 4mA to an external load. If the load of the THVD14X9 does not exceed that then you should be able to power it from the AVDD supply. Generally I would recommend using an external supply instead of the AVDD to avoid situations that might overload the regulator, since the AVDD is an important supply for internal blocks as well.
Regards,