Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443
I am using the IWR1443 boost sensor board. When I am trying to localize objects in a room without the clutter removal option enabled there is always a very high peak in the range profile around 3-30cm.
It seems like there are ghost points detected right in front of the sensor although there is no object infront of it. This peak in the range profil remains constant at approx 100dB even if I move the sensor away from or closer to an object.
Do you have any idea why this happens and how to counteract this phenomenon?
The image below illustrates the range profile peak around 3-30cm as it is seen in the mmWave Demo Visualizer.
I am using the following configuration generated by the Visualizer: