Hello, I am using a DRV5055-Q1 linear hall effect sensor as a gear tooth sensor for my application. The sensor has a bandwidth of 20kHz. The gear rotates at around 1500 rpm to 2500 rpm. i am unable to attenuate the noise generated. So i need to develop a Low pass RC filter as stated in the DATASHEET. which i did try but i am not very much satisfied and the result is poor. Can you help me with the required values of the R and C that i need to incorporate.