Other Parts Discussed in Thread: PGA305, PGA308, PGA900, DAC7760
In the case of pressure sensors bridges that swing positive and negative with respect to each other, with the application of positive and negative pressure (vacuum), does the PGA300, 308 and 900 DAC output a negative voltage when a vacuum is pulled on a Gauge pressure sensor? Also, is it flexible enough that when you have an absolute sensor (say 15 PSIA), where the low DAC voltage output of 0V will occur when you pull a vacuum on the sensor, and the high output voltage of the DAC (5V) will be when the bridge is nearly balanced at room pressure?
Lastly, how does is the 3rd order compensation accomplished when operating as described above?