I want to know PGA900 if the PGA900 has a digital output? for example: data output through I2C, SPI.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to know PGA900 if the PGA900 has a digital output? for example: data output through I2C, SPI.
Hello,
The PGA900 can output a digital value using the COMBUF registers. Please see the datasheet section describing "Accessing PGA900 Memories While Microprocessor is Running".
While the internal MCU is running, only a few registers are accessible via the digital interfaces. Some of those are the COMBUF registers. You can program the firmware to recognize commands that are sent to the COMBUF_DIF_TO_MCU register and output data on the COMBUF_MCU_TO_DIF register.
Regards,
Hello,
I2C and SPI are both interfaces that could be used for the combuf communication. The combuf is accessible via any of the available digital interfaces since they are just normal device registers.
Please refer to the SPI and I2C sections of the datasheet for more information on how to structure I2C or SPI data packets so that they can be processed by the PGA900.
Regards,