Hi,
1.
I found an pdf show the method on how to get ADC data by CCS debug
<<ADC Data Capture using Capture Demo and CCS Memory Browser IWR14xx/AWR14xx example>>
e2e.ti.com/.../ADC-Data-Capture-SDK1.05-V1.00.pdf
C:\ti\mmwave_sdk_01_00_00_05\packages\ti\demo\xwr14xx\capture
2.
In my environemnt
SDK:
mmwave_sdk_03_03_00_03
mmw
C:\ti\mmwave_sdk_03_03_00_03\packages\ti\demo\xwr68xx\mmw
3. I use ccs debug to capture ADC buffer as below:
3.1
I use ccs debug to load mmw binary
3.2
run mmw
3.3
then input the CLI with profile_2d.cfg(which is the standard cfg, on with change "frameCfg 0 1 32 1 100 1 0")
after the profile_2d.cfg is done, one frame is done.
3.4
then I use CCS Memory Browser to save ADC (it is the ADCdataBuf's address 0x52000000 in mmw)
4.
Is Item3 Correct? Becasue my SDK is 3.3 and app is mmw.
Thanks
PCD