Other Parts Discussed in Thread: IWR1642
For IWR1642, the maximum range is determined as 80m. I loaded the Driver vital signs image into the ti mmwave radar and got the maximum range to be around 105cm.
In the below URL, under 'Configuring the GUI' section, it was mentioned that the max range is only 0.7m.
Can someone please tell me how to modify the range to its maximum range while using the Driver vital signs application.
I appreciate the response.
Thanks,
Ramya