I was working on lab using the TI-RSLK Max Kit and when I tried using the slide on/off switch on the chassis board, it came off. The robot still seems to run when I used the debugging software however a possibly defective on/off switch is concerning. I would like to know if the chassis can be replaced before I have to order another robot kit. I would have put a part number in this post but I could not seem to find one that this site recognizes.
Below is the a picture of where the switch broke off: