Hi,
Customer created a system using TS12A12511 with input switching.
They are using TS12A12511 under Vcc = 5V, -Vcc = 4.5V conditions.
When connecting a signal to this set, a transient voltage below -Vcc is applied temporarily.
Let me ask you three questions about negative voltage transients.
1.
Data sheet states that the absolute maximum rating of the voltage applied to NC, NO, or COM is -Vcc-0.5V.
From this specification, it is presumed that an ESD protection diode is provided between the NC, NO, or COM terminals and -Vcc.
However, when observing the input signal waveform, the voltage is not clipped to -Vcc-0.7V.
Is there a protection diode?
2.
If a protection diode is installed,
Maximum input current II / O specified by the absolute maximum rating in the data sheet is Continuous current NC, NO, or COM ± 50 mA.
Will the device be damaged even if ± 50mA is constantly generated in the protection diode?
In addition, there is Peak current NC, NO, or COM ± 100 mA, but momentarily, it will not break even if 100 mA flows.
Is this understanding correct?
Also, how long do you expect the duration time of the peak current?
3.
On the other hand, from the viewpoint of voltage, a transient of -8V is generated.
Is there a time limit for voltage transients?
Please let me know if there are any of the following rules.
Best regards.
Yusuke