Other Parts Discussed in Thread: TMUX1511, SN74CB3Q3125, , TS5A23166, TMUX1574, TMUX1575
Hi There,
I am thinking use this part to isolate the signals between two power domain, battery (3.0V) and VCC-3.3V, the VCC may be powered off in some case and without isolation the battery will be consumed more leakage current through ESD diodes at VCC domain. Simple block diagram is as below.
the leakage current on powering off listed at datasheet is with condition of VNC and VCOM up to 3.6V, see capture below, do you have the leakage data on condition of 0 - 3.0V at VNC and 0V at VCOM for example.
another question is which pin of NC or COM is better to connect to battery domain signals?
the TMUX1511 is a better fit to me, but it's non stock on market. do you have other parts suggestion for my application?
Thanks
Bo