Hello,
Customer is looking for a new bus switch with 2 channels for low-speed signals such as I2C.
Do you have any good products other than SN74LVC2G66?
Best regards,
DDdoor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Customer is looking for a new bus switch with 2 channels for low-speed signals such as I2C.
Do you have any good products other than SN74LVC2G66?
Best regards,
DDdoor
Use the search function (here for 3.3 V):
ti.com/switches-multiplexers/analog/products.html#p1143=1:1%20SPST&p480=2&p3306=3.3
There is nothing wrong with the SN74LVC2G66. Which of its characteristics do you want to improve?
Hi DDoor,
As Clemens has stated, the current device you have selected works just fine for I2C. Is there a specific feature or electrical specification that the customer is after in their design?
You can access the product page for analog switches and multiplexers here. Using this link, filter on the left-hand side by 1:1 SPST and 2 channel. This will give the same configuration as the SN74LVC2G66.
The TMUX1121 is 1.8V logic compatible, has built in fail-safe logic, and implements break-before-make switching. There is also a wide supply of this device available on TI.com compared to other TMUX devices, so it should be readily available if you want to purchase this device.
Regards,
Tyler