Hi,
My customer designs TPS5A3157 for eSPI application, however, 1.8Vcc cannot work, but 3.3Vcc is OK.
Schematic and waveforms are shown below. Why cannot work at 1.8Vcc?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer designs TPS5A3157 for eSPI application, however, 1.8Vcc cannot work, but 3.3Vcc is OK.
Schematic and waveforms are shown below. Why cannot work at 1.8Vcc?
Hi Alan,
It looks like they have 0ohm resistors between the channels, can the customer remove the mux and confirm the circuit works when directly connected?
For the 3.3V case, can they provide similar waveforms as the one they provided for the 1.8V case? The TS5A3157 should work at both voltage levels without issue.
Thanks,
Tyler